(0)| 5/15/2018 1:45 PM | |
|
Joined: 8/3/2009 Last visit: 12/19/2025 Posts: 16612 Rating:
|
Hello The FWX-File is generated in a specific Version (for example WinCC flexible 2008 SP5 -> V1.5.0.0) If you want to open such a file for example with a WinCC flexible Runtime 2008 SP3 then its is not possible and you will get an error Message. -> Do you know which Image Version is on the real Panel installed? then you can look which WinCC flexible RT Version you need: https://support.industry.siemens.com/cs/ww/en/view/21742389 Bye Murof |
Last edited by: Murof at: 5/15/2018 1:47:47 PMIf this Information really helps, you could use the Rate function |
|
Follow us on