(0)| 1/13/2015 9:17 AM | |
|
Posts: 1368 Rating:
|
Hello, if you use two media converter in a line (SCALANCE X101-1 and the other switch) the TL (Tranparent mode) must be enabled (LED on). This can be done with the SET Taster. Have a look here in chapter 3.8 http://cache.automation.siemens.com/dnl/zA/zA0MTAzMQAA_22446594_HB/BA_SCALANCE-X100-MC_76.pdf NOTE A direct cascading of two SCALANCE X101-1 FL or AUI is not possible! Good luck! |
| 1/14/2015 8:23 AM | |
|
Posts: 11 Rating:
|
I am sure that the reason is the speed of the FO. Is there any scalance whose FO velocity is 1000MB/s??
|
| 1/14/2015 9:24 AM | |
|
Posts: 1368 Rating:
|
Hello, all SCALANCE use - as I know- 100MBit/s for FO Port... |
Follow us on