(0)| 7/30/2015 5:18 PM | |
|
Posts: 66 Rating:
|
Hello I tried to install TIA Portal V13. I could install the following packages successfully: STEP7 PROF V13, STEP 7 PROF SP1 V13.0, and WinCC V13 PROF. However, When I installed WINCC V13 PROF SP1 an error showed up moreover I'm working with a Virtual Machine VMWare with Windows 7 Professional 64 bits SP1. The error is: 12:46:24 | OK RebootAfterAll SetupUnit (SCADA-RT), Complete - - PlusMain, Reinstall 12:46:34 |ERROR SeconWorker::ExecuteSeconWork(): - Secon call has been finished with errors 12:46:34 | FAIL! SecurityControl (SCADA-RT), Failed;After I attached the log file created after the installation.
AttachmentSIA_WINCC_PROFESSIONAL_V13_SP1@15-07-10_11-42-19_summary.txt (387 Downloads) |
Last edited by: Min_Moderator at: 7/31/2015 9:11:19 AMNew subject after splitting |
|
This contribution was helpful to
|
|
| 7/31/2015 9:12 AM | |
|
Posts: 4758 Rating:
|
|
This contribution was helpful to
|
|
Follow us on