(0)| 11/17/2015 11:50 AM | |
|
Joined: 11/15/2015 Last visit: 12/3/2025 Posts: 180 Rating:
|
HELLO DEAR i have siemens milltronics BW500 belt weighing system ...i have done some mistake on the program parameters ....( P367-1 Direct Zero Entry Enter zero count 0 i have enter the zero ) & (P368-1 Direct Span Entry Enter Zero count 0 i have enter 0) the last values was ( 55543 / and value around this i could not remember it ....i want to return to the run menu but i could not ....i have reset the power the system initial up not completed (system check 1..2...3...4..5..6..7) and stop at this ( system check 7) please help me for solve this problem ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 11/17/2015 2:34:47 PMNew subject after splitting Look for alternative not for the correct answer...if this is helping you rate it. |
|
Follow us on