(2)| 3/29/2016 10:22 AM | |
|
Posts: 66 Rating:
|
Dear friends, i was reading this article How can I get an overview of the S7-400 memory concept? but one point i could not understand which is: "Do you wish to be able to change the user program in RUN mode, and is the program too big for the internal RAM? If so, this would necessitate the use of a RAM memory card. When using a RAM memory card, the system must be battery-operated so as to back up the RAM memory card data and the data in the internal RAM if there is a power failure." This means if i use FLASH memory card i will be not able to change the user program in RUN mode. ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 3/30/2016 9:42:44 AMNew subject after splitting |
|
| 4/19/2016 1:11 PM | |
|
Joined: 4/28/2015 Last visit: 11/27/2025 Posts: 10970 Rating:
|
Hello, look at this article, hope it shows you what you want: |
|
With best regards... |
|
Follow us on