(0)| 5/24/2016 3:00 PM | |
|
Posts: 3 Rating:
|
Hi everyone I am facing a problem in profinet network in which I have a CPU 315-2PN/DP which is communicating to 4 NX100 yaskawa controller and 1 MP HMI through scalance x208. The problem is after some time the scalance module goes in the fault mode and its fault LED remains on solid red, on the other hand CPU X1 port led which remains solid yellow when communicating, goes to off state. When i recycle the power of the scalance and CPU than problem fades away but it keeps on repeating after some time. Is the scalance unit faulty as when i diagnose it on hardware diagnosis of 315 it call OB86 i/o access error and shows the i.p. address of scalance. Any help in the regard would be highly appreciated. ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 5/25/2016 9:29:14 AMNew subject after splitting |
|
Follow us on