(0)| 6/28/2016 12:04 AM | |
|
Posts: 16 Rating:
|
Hi,
L MD10 ITD DTR L 300.0 /R L27648.0 *R RND T PQW128 I am able to generate the signal. But when i give ma signal to the display unit. for 300 it displays - - - - overflow. for 150 it displays 5000. My question is how to make it display 300 when i load MD10 with 300 or how to make it display any number i write to MD10. I am using CPU314IFM. I have attached the pdf of the display unit. its a calibration pdf. the model number is DA10-NA40/E10R. I have put min display value to 0000 and max display value to 9999. also min internal signal to 0000 and max internal signal to 20.00.
Thanks, ------------------------------------------------------------------------------------------ AttachmentDA10NA calibration.PDF (187 Downloads) |
Last edited by: Min_Moderator at: 6/29/2016 12:21:54 PMNew subject after splitting |
|
| 7/7/2016 10:39 AM | |
|
Posts: 16 Rating:
|
Thanks a lot Piotr.M. The unscale function was much more accurate in giving a reading matching to that of the PLC. |
Follow us on