(0)| 5/4/2017 5:18 PM | |
|
Posts: 5 Rating:
|
I have an AFE rectifier, which is responsible for powering the hoist / gantry inverter. However, the fault only occurs when the drive is being reconnected after a period of time off. That period is short! F009, after recurrence causes failure f004. After several attempts, the failed equipment does not return and the equipment operates until the end of the shift normally. Any idea of what might be causing it is flawed? Type: 6se7141-5ba0-z Parameters: p071: 400 P074: 65 % P155: 100 ms r949: 20 ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 5/5/2017 2:19:06 PMNew subject after splitting |
|
| 12/3/2021 7:56 PM | |
|
Posts: 6 Rating:
|
Hello I have similar problem in my drive ( with hoist and gantry application on crane ). How do you solve problem? Thank you. Saman1361 |
Follow us on