(0)| 6/18/2017 9:19 AM | |
|
Joined: 4/22/2014 Last visit: 2/16/2025 Posts: 20 Rating:
|
Dear Experts, I am having an issue with FB5 Sample_T parameter. As you know, the default Sample_T for FB5 is 1s. All my FB5 blocks previously were in OB1 with default Sample_T of 1s. Recently i have moved all the FB5 blocks to OB35 (100ms) task and also did a complete donwload to my S7400 416-3 PLC due to some hardware changes done. After the download, surprisingly in all the FB5 blocks i could see that the Sample_T has changed to 0.1s. It would be great to know if someone had come across similar issue or knows more details about it. I am using PCS7 V8. The FB5 block i have used from ELEMENTA PCS7 library. Best Regards, Ram Kishore ------------------------------------------------------------------------------------------ |
Last edited by: Ram_BahrainSteel at: 6/18/2017 9:22:06 AMLast edited by: Min_Moderator at: 6/20/2017 6:14:04 PMNew subject after splitting |
|
Follow us on