(0)| 7/4/2017 11:54 PM | |||||||||
|
Posts: 1 Rating:
|
Currently I am working on Sinamics Power Module (6SL3351-1AE32-1AA2) having control unit CU 320 (6SL3040-0MA00-0AA1).I want to run this unit using BOP. For this purpose I have to made these parameters settings along with other motors data setting
When I edit these parameters (for example writing r0019.0 to P0804 [0]), these are not changed .Also upon factory setting these values are not changed so what should I do?At this time no control wiring is attached to control unit 320 so upon power up its showsF07860External Fault 1 ------------------------------------------------------------------------------------------ |
||||||||
Last edited by: Jen_Moderator at: 7/10/2017 8:32:39 AMNew subject after splitting |
|||||||||
Follow us on