(2)| 1/18/2018 6:38 PM | |
|
Joined: 10/26/2011 Last visit: 12/23/2025 Posts: 766 Rating:
|
Hello GregVand7, in the manual "CFC for SIMATIC PCS 7" you find all the information about the CFC: In the chapter "Indroduction" you get an overview about CFC: |
|
SIMATIC PCS 7 - Overview |
|
This contribution was helpful to
|
|
| 1/18/2018 6:55 PM | |
|
Joined: 10/26/2011 Last visit: 12/23/2025 Posts: 766 Rating:
|
Yes, CFC is only for PCS 7. It is most easier to write the program new. CFC is very simple to use. If you engineer you program in CFC, the associated picture symbols and faceplate are For beginners, Siemens provides a very helpful and easy Getting Started. The most functionalities for basic engineering are explained. With several step by step instructions, you learn more and more about PCS 7 and by the way you are engineering your first small project, called Colour Project. At the end you have a color mixing plant, with two tanks, which you can operate in the OS Runtime (no real CPU is needed; only PLCSIM). PCS 7 Getting Started - Part 1 (with APL) PCS 7 Getting Started - Part 2 (with APL)
|
|
SIMATIC PCS 7 - Overview |
|
| 1/18/2018 7:51 PM | |
|
Joined: 3/14/2008 Last visit: 12/28/2025 Posts: 2233 Rating:
|
Thunderstorm, Option package: CFC is also released for Step7, it is not only valid for PCS7!
|
|
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to
|
|
| 1/18/2018 8:33 PM | |
|
Posts: 2 Rating:
|
Thanks for your replies ! So, is the use in PCS 7 (automatically associated symbols) the biggest interest of the CFC ? |
Follow us on