4/3/2019 11:19 AM | |
Joined: 6/29/2018 Last visit: 8/28/2025 Posts: 23 Rating:
|
DCC interconnection with SINAMICS parameters: r21001 does not show up Now there is another question: I would like to consider the execution period of my DCC chart inside the calculations. It is the parameter r21001[0] and I want to connect it to a Mul input. However, it does not appear in the "DCC Signal Selection" window. (Compare DCC Editor Description chapter 4.1.3.7). The offered parameters end with r9733. No higher parameter numbers offered. ------------------------------------------------------------------------------------------ |
Last edited by: Papa123 at: 4/3/2019 11:20:35 AMLast edited by: Jen_Moderator at: 4/3/2019 1:01:31 PMNew subject after splitting |
|
Follow us on