(5)| 6/17/2021 9:56 PM | |
|
Joined: 9/23/2005 Last visit: 1/6/2026 Posts: 4438 Rating:
|
Hi,
They could be changed in runtime (for example for “Night light” event or user preferences) by scripting:
sample project AttachmentUni21_20210617_1654.zip (1365 Downloads) |
Last edited by: Denilson Pegaia at: 01/09/2024 09:54:51Denilson Pegaia |
|
This contribution was helpful to
|
|
| 11/10/2021 11:34 AM | |
|
Joined: 9/23/2005 Last visit: 1/6/2026 Posts: 4438 Rating:
|
Hi, here tere is an exemple of a button that read the actual style and save it in an internal tag. AttachmentUni21_20210617_1654_20211110_0731.zip (1485 Downloads) |
|
Denilson Pegaia |
|
This contribution was helpful to
|
|
| 1/9/2024 10:05 AM | |
|
Joined: 9/23/2005 Last visit: 1/6/2026 Posts: 4438 Rating:
|
Hi As from TIA V19, unlike WinCC Advanced (https://support.industry.siemens.com/forum/br/pt/posts/tip-wincc-v13-hmi-style-editor/105979/?page=0&pageSize=10) where the styles are configured inside TIA, WinCC Unified styles are edited in a separate tool, Corporate design, available at https://support.industry.siemens.com/cs/br/en/view/109824234. This allows, among other things, for styles to be developed by design specialists, on separate computers, for example. On this page are available:
Configuration steps
TIPs: "Notes on use IO field The IO field does not use a rendering template from the user-defined style in TIA Portal and Unified Panel. The user-defined rendering template is used properly during display in the Unified PC Runtime and simulation. Font settings Font settings "Italic", "Underlined", "Strikethrough", which are configured in a user-defined style, are lost both when importing to TIA Portal and when importing back to the Corporate Designer. Saving, closing and reopening the project It is recommended to save the project in the Corporate Designer, then close and reopen it before changing the assigned color palette or font group for one of the styles in the project. You import the corporate design file into the WinCC Unified Engineering System. You download the defined style items to Unified PC, Unified Comfort Panel and Unified Basic Panel and use them in the screens of your TIA Portal project." Sample project (archived from TIA Portal as .zap19 and after that compacted in .zip format to be uploaded here) user= User, all password = Password1! Attachmentproject style.zip (919 Downloads) |
Last edited by: Jen_Moderator at: 01/10/2024 08:17:44Text formatting optimized. Denilson Pegaia |
|
| 1/10/2024 12:30 PM | |
|
Joined: 2/11/2020 Last visit: 12/15/2025 Posts: 14 Rating:
|
Hi, How can we use it in multiuser project? How add the file into project on server? |
Follow us on