8/14/2018 9:36 AM | |
Joined: 8/3/2009 Last visit: 9/19/2024 Posts: 13735 Rating: (1730) |
Hello Yanto you have to set the PGPC Settings in the Runtime PC. -> Control Panel -> set view to small icons-> Set PGPC Settings -> set here the S7ONLINE Access Point to your Networkcard.tcpip.1 And if you run only the WinCC Flexible RT on thePC you do not need a PC Station Konfiguration with Simatic NET. Here is a FAQ for all the possible Ways of configuration: https://support.industry.siemens.com/cs/ww/en/view/24109937 Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on