8/13/2017 9:33 AM | |
Posts: 3 Rating: (0) |
hi sir how can i do upload s5_95u profibus network or changed the station spacial code? whats windows i need? thanks for your guide ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 8/14/2017 8:30:16 AMNew subject after splitting |
|
This contribution was helpful to1 thankful Users |
8/13/2017 1:40 PM | |
Joined: 9/27/2006 Last visit: 4/18/2024 Posts: 12256 Rating: (2664) |
Hello abolfazial; The oftware required to configure the Profibus network on a S5-95U is COM Profibus. Here is a manual that you can look at: com profibus - Siemens Support I have worked with versions 3.3 and 5.0. Neiuther version is on the market at this time, I suggest you contact Siemens to locate the file. The command to upload an existoing cnfiguration is "Device-Import". Hope this helps, Daniel Chartier |
This contribution was helpful to1 thankful Users |
8/17/2017 2:43 PM | |
Joined: 9/27/2006 Last visit: 4/18/2024 Posts: 12256 Rating: (2664) |
Hello abolfazlasi; This is a note I posted in a similar thread to yours, yesterday: Edit: COM Profibus v5.1 is, surprisingly, still listed in the Siemens Industry Mall (Electronic catalog): https://mall.industry.siemens.com/mall/en/us/Catalog/Product/6ES58956SE03 The datasheet attached is dated "last modified: 08/12/2017"; so even in phase-out it seems to be available from Siemens. You should try to contact a Siemens rep. and check out the pricing, base don the part number. D.C. Hope this helps, Daniel Chartier |
8/22/2017 6:15 AM | |
Posts: 3 Rating: (0) |
hello daniel chartire thanks a lot for your helping. i will check and do upload/download over other cpu and when i do safe so i connect the network and chenge the program. i willnot connect siemens agency because it isnot available any time. thanks for your guide. abolfazl aslnezhadi
|
Follow us on