8/21/2017 8:43 AM | |
Joined: 4/8/2016 Last visit: 8/30/2024 Posts: 133 Rating: (45) |
Hello bormotor, as far as I know the S7-300 CPUs are not released and not suitable for PCS 7, thus the CPU 315-2DP is not included in the requirements for PDM in PCS 7. Here is the FAQ with the requirements for PDM routing, which gives you an overview over the ES/AS components supported by PCS 7: https://support.industry.siemens.com/cs/ww/en/view/7808062 But back to your question, if it will work. In another FAQ (not PCS 7 specific) I found that the CPU 315-2DP supports data record routing for PDM but the CP 343-1 apparently does not: https://support.industry.siemens.com/cs/ww/en/view/7000978 |
Kind regards |
|
This contribution was helpful to2 thankful Users |
8/22/2017 7:50 AM | |
Posts: 2 Rating: (0) |
Thanks a lot. Very helpful. |
Follow us on