10/17/2017 10:12 AM | |
Posts: 80 Rating: (1) |
Hi All, I make a test with D435-2DP with S120. I make a MCC chart named as MCC_Test and assign in task Motion 1. The MCC_Test serves to change speed of followingAxis from 2 Virtual Master. Anybody can look into the MCC chart and give some comments? fyi, i am using Scout v4.5 Thanks. Azad AttachmentSample_1_1.zip (48 Downloads) |
10/17/2017 10:55 AM | |
Joined: 5/12/2006 Last visit: 4/26/2024 Posts: 22231 Rating: (2980)
|
Hi, any error message during the execution? which on is working and which one not? |
Follow us on