3/14/2018 1:42 PM | |
Posts: 5 Rating: (0) |
Hello I have a pretty bad problem with generating modul drivers in PCS7 9.0. My Hardware Configuration: I am using SIMATIC PCS 7 CPU 410 redundacy automation system (2x CPU 410-5H). I have 11x switches (I am using SCALANCE XF204-2 and SCALANCE XF204-1). I have 6x IE/PB LINK PN IO Gateway (each link has it's own profibus). I have around 56x IM155-6PN-HF-V3.1 on ethernet. I have 7x SINAMICS G120 CU230P-2 DP V4.7 on IE/PB LINK's profibus. I added one DI8x24VDC ST V1.0 for testing to IM155-6PN-HF-V3.1. And finally, I am using around 108x SIMOCODE pro V (GSD V1.5) on IE/PB LINK profibuses. I made all necessary connections in Profinet IO Topology through a Graphic view. Compilation of my Hardware Configuariton was successful. I have no software there yet. When I create a CFC, find a Pcs7DiIn driver in Libraries - PCS7 AP Library V90 - Blocks - Channel, add one driver block to my CFC with address digital connection (corresponding to my digital card) and try to compile the project an error of generate modu driver will occur. What is curious about the error is, that I always get a little different error log in Module driver folder and also the number of errors is changing each compilation (I was not changing anything during all these test compilations). Sometimes it goes up and sometimes down. More info about error logs in the attachment.(there are two compilation logs in this file) I will appreciate all responses. EDIT: So when I delete all IE/PB LINKs with profibuses from Hardware Conf, it works. I will have to find out what exactly is causing that. AttachmentSIMATIC H Station_Module driver.txt (188 Downloads) |
Last edited by: Morvis110 at: 3/14/2018 2:17:31 PMLast edited by: Morvis110 at: 3/14/2018 2:18:10 PM |
|
3/15/2018 12:58 PM | |
Posts: 5 Rating: (0) |
It appears, that when I have more than 10 SIMOCODES PRO V in one IE/PB LINK's profibus, then I start getting these errors. Anyone knows why? |
Follow us on