8/14/2018 12:35 PM | |
Posts: 13 Rating: (0) |
Hello, Does anyone has solution to this situation: S7-1200 is connected to internal network [snip]. When I connect [snip] everything is OK. But when we do connection from external network through router IP 84.17.558.58 (inside this router is opened port 443 for IP [snip]) https://84.17.558.58/awp/login/login.html we receive different errors which depends on browser (ex.:ERR_SSL_SERVER_CERT_BAD_FORMAT; DLG_FLAGS_SEC_CERT_CN_INVALID and etc.). The problem is that sertificate is created for IP [snip] and when we connect through router IP's mismatch and browser shows errors. p.s. port 80 is taken for others connections. Thanks. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 8/15/2018 7:22:04 AMBlanked out IP. Last edited by: Jen_Moderator at: 8/15/2018 7:23:34 AMNew subject after splitting |
|
Follow us on