11/13/2013 8:35 PM | |
Joined: 10/3/2008 Last visit: 9/8/2025 Posts: 996 Rating:
|
Hello, a new Modbus product is available now: "SIMATIC Modbus/TCP PN CPU Redundant" with the order number 6AV6676-6MB10-0AX0. With this product it is possible to establish a redundant communication with PN H-CPUs to third-party devices for transerring data via Modbus/TCP. A single-sided redundancy and/or a double-sided redundancy is possible. Same like in the other Modbus products Holding Register, Input Register, Coils and Inputs (function codes 1, 2, 3, 4, 5, 6, 15 and 16) are supported. The demo version and the manual are downloadable here: www.siemens.com/s7modbus. Wüstenräuber |
This contribution was helpful to
1 thankful Users |
11/25/2013 2:51 PM | |
Joined: 10/3/2008 Last visit: 9/8/2025 Posts: 996 Rating:
|
Hello, the wizard for "Modbus/TCP PN CPU Redundant" is downloadable here: www.siemens.com/s7modbus, tab "Downloads". Wüstenräuber |
5/2/2014 7:16 AM | |
Joined: 1/9/2012 Last visit: 8/12/2024 Posts: 40 Rating:
|
Canthis libraryused with STEP 7 V5.5 SP3? |
5/2/2014 7:35 AM | |
Joined: 10/3/2008 Last visit: 9/8/2025 Posts: 996 Rating:
|
Hi Dnyanesh, yes, it's released for this STEP7 version. Wüstenräuber |
This contribution was helpful to
1 thankful Users |
5/2/2014 7:58 AM | |
Joined: 1/9/2012 Last visit: 8/12/2024 Posts: 40 Rating:
|
Regards, Dnyanesh |
3/30/2016 8:27 PM | |
Joined: 9/3/2008 Last visit: 8/19/2025 Posts: 938 Rating:
|
Hi Atul, Use the link given in the previous posts: Then from that page, in the right-hand side open the "Support" option and click the "Software downloads" link. |
Michael |
|
9/30/2019 9:49 PM | |
Joined: 9/1/2005 Last visit: 8/22/2025 Posts: 4114 Rating:
|
New question published by AutoGen_656847 is split to a separate thread with the subject trying to figure out can we write our own protocol using the RS-485 builtin interface on S7-300 or S7-400 Cpu's. Best regards |
My Forum is the place to personalize your profile, |
|
Follow us on