(0)| 4/5/2014 8:59 PM | |
|
Posts: 895 Rating:
|
Hello, I suppose SIEMENS will sell SINAMICS S for common DC- bus. From technical view I should work like Micromaster (but notPM240-2 Framesize A): http://support.automation.siemens.com/WW/view/de/22093973 Maybe you can discuss this with your SIEMENS sales partner. I think it`s more a topic because of EMC. Further SIEMENS would have to do a systemtest for a combination where a S120 booksize combination would be a good solution. Zako |
| 4/5/2014 9:28 PM | |
|
Joined: 11/21/2007 Last visit: 1/8/2026 Posts: 2327 Rating:
|
Hello zako_ Thanks for your insight. If this was possible with MM440 ( As is clear from the link that you posted ), I would be surprised of G120 ( PM240 ) does not support his. After all G120 is supposed to be the next generation drive after MM4 ... We frequently use S120 on common DC Bus, but cost limitations do not allow us to use S120. Cheers Navnag |
|
There is no such thing as the last bug in a program |
|
| 12/3/2014 4:36 PM | |
|
Posts: 1 Rating:
|
What is your concern and reasoning behind not being usable with PM240-2 Frame A? |
Follow us on