8/19/2014 10:07 PM | |
Joined: 4/6/2014 Last visit: 9/24/2022 Posts: 7 Rating:
|
why start simulation not active that shown in picture when I want to simulate offline without real PLC |
8/21/2014 9:40 PM | |
Posts: 5225 Rating:
|
Thank you for the pictures, those are really helpful. As huggy_d1 said the S7-1200 PLC does not simulate, but the S7-1500 can simulate. Roughly the steps:
There is no need to create any secondary device inside TIA. TIA responds as if the PLC is actually connected. In actual fact TIA is connected to the PLCSIM software. Need more detail?.. is it helpful? [2015-04-30] |
Last edited by: William_B at: 4/30/2015 2:27:08 PMAdd an update note after user thanked for posting. |
|
This contribution was helpful to
5 thankful Users |
5/9/2015 2:37 AM | |
Posts: 47 Rating:
|
Thank you |
Follow us on