9/10/2014 2:23 PM | |
Posts: 1368 Rating: (126) |
Hello, have a look on this faq http://support.automation.siemens.com/WW/view/de/18005211 |
9/10/2014 5:51 PM | |
Joined: 1/3/2006 Last visit: 2/19/2024 Posts: 726 Rating: (71) |
Hi Felman Even if maximum connection possible is 32 for 317, number of simultaneous connections is limited to 16. And I guess you are using 16 simultaneous PUT instructions using 343-1 Advanced. What it means is that at any given time not more then 16 communications can be underway. More details overhere. Regards Manmeet |
9/11/2014 8:33 AM | |
Posts: 1368 Rating: (126) |
hello I agree with manmeet |
9/11/2014 1:33 PM | |
Posts: 1368 Rating: (126) |
In TIA, you must use GET_S. With this, you can use the integrated PN Interface of CPU or CP look here https://www.automation.siemens.com/mdm/default.aspx?DocVersionId=63972520715&Language=de-DE&TopicId=53480313739 |
This contribution was helpful to4 thankful Users |
Follow us on