12/2/2014 2:01 PM | |
Posts: 1058 Rating:
|
Hello sma_1000, when IM151 is connected as pb-slave, it cannot recognice other conneted modules. Termination of profibus is always on first and last node on bus. Maybe these links can be helpful for setting up IM151. How do you read out the diagnosis data of a PROFIBUS DP slave with the SFC13 "DPNRM_DG" and how do you evaluate the data in the user program? Which diagnostics messages might you get when commissioning the ET 200S as PROFIBUS DP slave? SIMATIC Distributed I/O Product Information for the ET 200S IM 151-1 STANDARD, IM 151-1 HIGH FEATURE Manuals SIMATIC ET 200S distributed I/O IM151-1 STANDARD interface module (6ES7151-1AA05-0AB0) regards |
Follow us on