(0)| 3/19/2015 7:45 PM | |
|
Posts: 1 Rating:
|
Hi, I have an issue with the MultiRanger 100 too. I have a pump pumping liquid into the top of a tank. When the pump is not running the level reading is accurate. Once the liquid is being pumped in to the tank the level jumps up to ~90% as if the sensor is picking up the flow of the liquid in to the tank. The sensor is located at least 2 meters away from the location of the pipe. Is it possible to reduce the width of the scanning area so that the sensor does not pick up the flow in to the tank and only sense liquid directly under it? Thanks
---------------------------------------------------------------------------------------------------- |
Last edited by: Min_Moderator at: 3/20/2015 10:33:21 AMNew subject after splitting |
|
Follow us on