(0)| 4/15/2015 11:38 AM | |
|
Posts: 1 Rating:
|
Dear Sirs., I have he same problem (NOx value is *********) and in the log it says that the autocal drift beyond tolerance, but that is not true. I have a drift of 1-2% and the limit is 10%. like in the following post: https://support.industry.siemens.com/tf/ww/en/posts/ultramat-23-no-gas-reading-after-autocal/67547/?page=0&pageSize=10 We have 2 Ultramat 23 and it happened in both already. The first one was replaced by the Siemens warranty, we got a new equipment, but now for the second one the warranty is over. How do I know if the problem is with the IR Source, the CH4 detector or contamination of the analyzer cell? Thank you in advance
|
Last edited by: Min_Moderator at: 4/15/2015 4:22:16 PMNew subject after splitting |
|
Follow us on