4/17/2015 12:37 PM | |
Posts: 18 Rating: (2) |
1)I am using profinet communication for cpu 315-2pn dp with IM 151-3pn.I am using profinet communication for cpu 315-2pn dp with IM 151-3pn. There are 10 IM modules communicating with 315 cpu. For one im module i am facing one problem. Everytime when i remove profinet cable or at the start of day when i power up the panel the IM module goes into bus fault.After the communication breaks with cpu 315 after that i need to power off the IM 151-3pn to remove the bus fault.But the rest of the IM 151-3pn are working fine after the communication is healthy at the start of day or after removing profinet cable.Only one IM I am facing the issue.Is any parameter I have to change or this issue is due to hardware configuration or something else i have to look for? 2) ... [snip] sorry for bad english.I am in site for commisioning please give some suggestions. ------------ |
Last edited by: AKHIL SADANADAN at: 4/17/2015 12:39:18 PMLast edited by: CS Moderator at: 4/19/2015 10:42:59 PMnew subject after splitting |
|
Follow us on