(0)| 5/7/2015 9:42 AM | |
|
Posts: 30 Rating:
|
The doubt is how to make invisible a reference panel inside one faceplate. I have make this script in the initialize of the faceplate: main() { dpConnect("visibilidad","EBAB_IZ01_SB_B_001.E.local:_address.._active","EBAB_IZ01_SB_B_001.E.remote:_address.._active"); } visibilidad(string variable, int valor, string variable1, int valor1) { if (valor == 1) PANEL_REF3.visible(false); else if (valor1 == 0) PANEL_REF2.visible(TRUE); else PANEL_REF1.visible(TRUE);
This is not working, but if I make this with rectangles in the same faceplate they appears and disappears without problems. I think that the script is not able to access one reference panel and only access to real objects introduced in the faceplate. The reference panel I´m using is inside symbols_bool à stdlib_boolbutton1. With set value the problem is the same.
I hope you can help me. Thank you.
---------------------------------------------------------------------------------------------------- |
Last edited by: Min_Moderator at: 5/7/2015 5:19:20 PMNew subject after splitting |
|
| 5/7/2015 5:37 PM | |
|
Posts: 4757 Rating:
|
|
Follow us on