6/11/2015 1:54 PM | |
Posts: 2 Rating:
|
Hi everyone, I'm facing a problem in V20 for FAN application. When one of the three input phases is lost during running, the drive is not giving any alarm or fault. Is there the feature in V20 for line phase loss? And also when one of the three phases of motor is lost during running, VFD is not showing any alarm(A0922) is displayed but no Fault, the output current is falling to 80% of the running current. Some humming sound is observed in motor when one phase is lost. Can any one help me out...? Regards, Trinadh Babu.
---------------------------------------------------------------------------------------------------- |
Last edited by: AutoGen_981331 at: 6/11/2015 1:55:50 PMLast edited by: Min_Moderator at: 6/12/2015 12:11:51 PMNew subject after splitting |
|
Follow us on