(0)| 7/13/2015 11:25 AM | |
|
Posts: 1 Rating:
|
Hello, I want to create the HMI screen and Logic to view the Hardware Status at WINCC, I am using PCS 7 with S7-400 Redundant system. also need to know about SFC 51 Block, How to use it. i did not find it anywhere. The Only Available blocks in logic are SFC 6, SFC 20, SFC 64.
---------------------------------------------------------------------------------------------------- |
Last edited by: Min_Moderator at: 7/13/2015 3:40:41 PMNew subject after splitting |
|
| 7/14/2015 9:50 AM | |
|
Joined: 10/10/2014 Last visit: 12/8/2025 Posts: 1725 Rating:
|
Hello alburero, to view the hardware Status in WinCC you can use the Lifebeat Monitoring. Or for detailt PLC information you can use the WinCC Option SIMATIC Maintenance Station Best regards |
Follow us on