(0)| 7/14/2015 10:50 PM | |
|
Posts: 1 Rating:
|
Im using a s7-1200 cpu 1214 ac/dc/rly and a ktp600 conected via profinet (6ft long ethernet cable cat 6).The problem is that sometimes the values on the hmi are frozen and the equipment stops working without any alarm displayed in the ktp600, so i have to reset the power to work again, i would like to know why is this happenig, if its due to voltage variations or overloaded program, i have 2 screens to display the parameters of the system with like 8 or 9 analog tags each, with adquisition times of 500ms and 1s.
---------------------------------------------------------------------------------------------------- |
Last edited by: Min_Moderator at: 7/15/2015 11:28:04 AMNew subject after splitting |
|
Follow us on