(0)| 8/11/2015 10:20 AM | |
|
Joined: 12/17/2008 Last visit: 10/16/2025 Posts: 9 Rating:
|
I have S7-1200 with CM1243-5, so CPU1200 is Profibus DP master. Then I have IM 151-1 Basic with 2_SI module 4DF01, installed in ET200S rack. In HW Config this SI module gets hardware_ID 286. And now I want to communicate with partner thru ASCII protocol via RS485 line using this module. I use such call "SEND_PTP_DB"(REQ:="DB61". SendReq, //it is true while call "PORT":=286, BUFFER:="DB61".SendBuffer, //it is string LENGTH:="DB61".LengthOfRequest, //it is length of string upper DONE=>"DB61".SendDone, ERROR=>"DB61".SendError, STATUS=>"DB61".SendStatus); in status i get 7000 (block idle). Why idle? Can somebody say me what I am doing wrong? Is it possible at all to be CPU1200 as master in free ASCII communication? ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 8/11/2015 2:54:42 PMNew subject after splitting Last edited by: fatman at: 8/11/2015 2:55:39 PM |
|
Follow us on