(0)| 8/27/2015 6:24 PM | |
|
Posts: 10 Rating:
|
Hello, I need to synchronize Siemens Relays with Meinberg Lantime. I am using DIGSI v4.90. I set all the relays' Time Synchronization attribute to EthernetNTP. And then, created the IEC61850 Station added devices. After that, I imported sntp.icd into the same Network with the relays using the IEC61850 Configurator Tool. I set the IP address of the sntp device. But, some of the relays are synchronizing with Meinberg some are not. When I open the Time/date setting in the relay screen it says ST with the synchronized ones and says NS ER with not synchronized ones. I checked all the settings but there is no difference between settings. Can anybody help me, give me any idea? Thanks. I give the list of the relays with synchronising status below: 7SK8041 5EB903HE0 NOT OK 7SK8041 5EB903HE0 NOT OK 7SK8041 5EB903HE0 NOT OK 7SK8041 5EB903HE0 NOT OK 7SK8041 5EB903HE0 NOT OK 7SK8042 5EB961HE0 OK 7SK8042 5EB961HE0 OK 7SK8021 5EB901HE0 OK 7SK8021 5EB901HE0 OK 7SK8021 5EB901HE0 OK 7SK8042 5EB961HE0 NOT OK 7SK8042 5EB961HE0 OK 7SK8042 5EB961HE0 OK 7SK8042 5EB961HE0 OK 7SK8042 5EB961HE0 NOT OK 7SK8042 5EB961HE0 OK 7SK8021 5EB901HE0 OK ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 8/28/2015 10:04:31 AMNew subject after splitting |
|
Follow us on