9/17/2015 3:30 PM | |
Joined: 1/28/2009 Last visit: 10/11/2024 Posts: 6852 Rating: (1365)
|
Hello ,
The easiest way is to use SCL,Check a sample for a 2-dimension array HERE .The most difficult way is using STL in a loop.First, you need to calculate the absolute addresses of memories you are working and do a simple calculation (perhaps memory arrangement) to optimize using address regisers.Also you can find an STL solution there and compare. You are apparently working in an FB,is that right? I hope it helps, hdhosseini |
Follow us on