(0)| 10/7/2015 9:43 AM | |
|
Joined: 5/27/2008 Last visit: 1/5/2026 Posts: 29 Rating:
|
I' m facing the same problem. I have a running application on a IPC477. I can take over the WinCC Flexible RT Advanced via smartservice by entering: but sometimes when I try to connect, I get the following : "New connections disabled The requested resource is too busy to accept further incoming connections" =>I have to reboot the IPC to be able to connect via sm@rtservice again. =>Is there a way to resolve this without rebooting?
Remark: If I try to access the application via the sm@rtclient program (sm@rtaccess) at that moment, I still can connect to the application... ------------------------------------------------------------------------------------------ |
Last edited by: Maene3 at: 10/7/2015 10:15:47 AMLast edited by: Min_Moderator at: 10/7/2015 4:31:41 PMNew subject after splitting |
|
Follow us on