10/10/2015 10:31 AM | |
Joined: 8/23/2015 Last visit: 7/5/2025 Posts: 10 Rating:
|
please, any one can help me on Real time clock function about it's Basic and Concepts |
10/10/2015 10:46 AM | |
Posts: 8946 Rating:
|
Here is a fine link: https://support.industry.siemens.com/tf/ww/en/posts/31917/ |
This contribution was helpful to
1 thankful Users |
10/10/2015 2:37 PM | |
Joined: 9/27/2006 Last visit: 9/21/2025 Posts: 12420 Rating:
|
Hello Pawan; A real time clock (RTC) is a special electronic circuit designed to measure time accurately. It can be embedded in many types of devices, including PCs, radio and TVs, etc... Most modern PLCS and PACs integrate a RTC in their electronics. However, details of these circuits are not divulged by the PLC manufacturers generally. You will find instructions on reading and writing to it (for S7 CPUs, you should use SFC0 and SFC1 for this purpose) but you will find fee details on the circuit itself. If you open document #10 in IBN's list above (SIMATIC S7 CPU 31X TECHNICAL SPECIFICATION) you will find technical specs for the RTCs in the S7-300 family of CPUs. As an example, I have attached the details of the RTC of the S7-313C, as shown in that manual. Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 10/10/2015 3:15:56 PM |
|
This contribution was helpful to
1 thankful Users |
10/12/2015 1:53 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4759 Rating:
|
New question published by 9583815919 is split to a separate thread with the subject Switch on a output at 5 pm. Best regards |
Follow us on