11/20/2015 3:13 PM | |
Posts: 38 Rating: (0) |
Dear All, I have a problem with fwx file. I got a warning when I want to start runtime : " C:\.............\....\project_1.new.fwx configuration file could not be loaded. The application will be terminated. Because of this warning can not be started runtime. Please help me. Thanks a lot. ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 11/20/2015 3:45:34 PMNew subject after splitting |
|
11/30/2015 10:46 AM | |
Posts: 38 Rating: (0) |
As I understand if there is a problem with fwx file, when we load the program to panel we face the same problem on the panel. I faced ! Thanks in advices. |
11/30/2015 2:59 PM | |
Posts: 38 Rating: (0) |
Is the installed Runtime Package a SP2 or a SP3? ----> SP2 The FWX file is the compile resullt from WinCC flex, do you compile with SP2 or SP3?--->SP2 |
12/1/2015 9:40 AM | |
Posts: 38 Rating: (0) |
Could some one help me regarding this problem? |
Follow us on