2/20/2016 12:34 PM | |
Posts: 2 Rating: (0) |
Hello, I want to create a simple button that needs to work like this: - on left mouse click, it's tag is set to 1 and it's colour changes to green; - on next left mouse click, it's tag is set back to 0, and it's colour changes back to gray; I already managed to create the button and make it change a tag's value to 1 on left mouse click, but I can't figure how to make it change it's colour and that tag value back to 0 using the same mouse button. Can some one help me with this, please? ------------------------------------------------------------------------------------------ |
Last edited by: agb at: 2/20/2016 12:37:27 PMLast edited by: Min_Moderator at: 2/22/2016 4:44:30 PMNew subject after splitting |
|
Follow us on