(0)| 1/7/2008 8:39 AM | |
|
Posts: 32 Rating:
|
Hi I have looked in the Hardware (see Att) Is it the resolution the thinking about. And what about Preset value if you want to preset a kalibrationvalue on a specific hight on the position sensor. Is'it bit 2 in the lower byte?. Do you have an step 7 code for an exemple (FC or FB or STL ....) Attachmenthardw.zip (864 Downloads) |
| 3/17/2014 8:07 PM | |
|
Posts: 77 Rating:
|
Late reaction, But i was struggeling with this sensor last week i create an FB wich can be used if needed. AttachmentMTS_SERIES_R_DP.zip (1032 Downloads) |
| 8/18/2014 3:45 PM | |
|
Posts: 1 Rating:
|
Here is a simple way how to reset temposonic encoder. The M25.1 is "always-on" flag |
Last edited by: igorcris at: 8/18/2014 3:46 PM |
|
Follow us on