(0)| 4/1/2016 2:27 AM | |
|
Posts: 5 Rating:
|
Hello guys, today we had a problem in a MASTERDRIVES AFE we have in the company ( Quay Crane) , in order to perform control of AFE Hoist 2 (Slave) , and was going to 029 fails when the command is found off or logo after off it. As the fault manual indicates that it is a possible fault monitoring phase , probably carried out by CT . Therefore, use was made of Testbox MASTERDRIVE , and performed at the CTs offset measurement , and the related T phase ( L3 ) is with values above 1,500 M Ohms , while demics had between 80 and 90 Ohms . Even with this report, it has not been done to change the CT . The question is , the CU 029 has a failure , with no load equipment, ie , off ? How is this possible? Will could also be a problem with the IVI board, like a bad contact in your post , causing a bad feedback monitoring ? Thank you for attention. ------------------------------------------------------------------------------------------ |
Last edited by: Depaula at: 4/1/2016 2:29:48 AMLast edited by: Min_Moderator at: 4/1/2016 10:39:53 AMNew subject after splitting |
|
| 4/1/2016 11:02 AM | |
|
Joined: 8/31/2013 Last visit: 11/2/2025 Posts: 608 Rating:
|
Hello Could You tell Us the Type of MICROMASTER Drive |
|
Warm Regards |
|
Follow us on