4/1/2016 12:48 PM | |
Posts: 7 Rating:
|
First, Hi to all, I am beginner and new with PLC and have same problem with create datalog. I don't use real hardware, so first question is it possible to create datalog with testing program with PLCSIM? If it is posible, file should be stored in ProjectFolder/Logs? I read that plcsim doesn't simulate web interface, so didnt try it out. I use TIA V13 SP1, Step7Prof V13SP1 and WinCCProf V13SP1, CPU in project is 1214C firm. V4.1 I found in s7-1200 manual Example of Data log program, but still can't create datalog file. In attachment you can see my DB and program block. When i set create trigger bit, nothing happens. I try to find example of simple datalog, but find only example for v11, which i can't open with v13. Thanks for any help and sorry for bad English.
------------------------------------------------------------------------------------------ |
Last edited by: banezi23 at: 4/1/2016 2:14:31 PMLast edited by: Min_Moderator at: 4/1/2016 4:46:36 PMNew subject after splitting |
|
4/3/2016 3:43 PM | |
Posts: 7 Rating:
|
I found this example and figuered out how to retrive project in TIA v13, Sample Program: S7-1500 Data Log , so i can open this example sucessfully, but still can't create data log. When I trigger Create trigger M2.0. nothing happens. Am I missing something or i need some sequence to create datalog or ... So is it possible to create datalog without hardware? with PLCsim only? Anything, any idea would be helpful. Thanks, Banezi |
5/18/2016 3:24 PM | |
Posts: 7 Rating:
|
Hi Craig7, I do my best, but i couldn't figuered out how to make datalog. So I think that is not possiblewith PLCSim :) but still I am not sure 100%. Thanks, anyway. Regards, Banezi. |
Last edited by: banezi23 at: 5/18/2016 3:25:27 PM |
|
7/31/2018 4:17 PM | |
Posts: 3 Rating:
|
Hi, I am trying to do same thing as you. were you successful in creating datalogs? It would be great if you could provide me feedback. |
8/1/2018 6:16 AM | |
Posts: 7 Rating:
|
Hi, i didn't succeed to create datalog. I'm not sure 100%, but I think that i found in documentation manual that is not possible to create datalog with PLCSim. |
8/8/2018 9:40 PM | |
Posts: 3 Rating:
|
Thank you. |
Follow us on