(1)| 4/11/2016 5:52 PM | |
|
Joined: 2/19/2015 Last visit: 3/5/2025 Posts: 4 Rating:
|
Hello to all, Ì don`t understand nothing about profibus and i`m trying to setup a system where i have a s7 1200 1214 CPU as a slave using a CM1242-5. in all project i just need to exchange some data ( about 8 bits from the I\O port and some REAL values my question is in the configuration : do i need to create a Data Block with the data that i want to exchange and set as a path for the communication like in the MODBUS TCP \IP ? what kind of configuration i need to do? can someone help me? Kind Regards, Nuno ------------------------------------------------------------------------------------------ |
Last edited by: Blue Moderator at: 4/12/2016 7:41:00 AMNew subject after splitting |
|
| 4/13/2016 4:07 PM | |
|
Posts: 1410 Rating:
|
If you want to make a slave then all you have to do is configure I-slave transfer area in HW configuration of profibus slave module. You can R/W data from transfer area like R/W to input/output peripheral bytes/words of PLC. Look an example here: http://www.dynalogindia.com/wordpress/wp-content/uploads/2015/10/Moxa_Tech_Note-MGate5101_S7-1200.pdf |
This contribution was helpful to
|
|
| 4/14/2016 1:31 PM | |
|
Joined: 2/19/2015 Last visit: 3/5/2025 Posts: 4 Rating:
|
ohhhh... finnally i get it i think! thank you all for the support!!! With My best regards Nuno |
Follow us on