4/22/2016 2:20 PM | |
Posts: 6 Rating:
|
Hi, [snip] I got a new problem.. There is a cascade control where first loop is PID controller (vessel level)and the second is PI controller (flow). Second loop works fine, but level controller works tis way: set point 10%, controller drives level to 5% set point 20% controller drives level to 10% set point 30% -.- 15% set point 40% -.- 20% set point 50% -.- 25% set point 60% -.- 30% set point 70% -.- 30% set point 80% -.- 30% set point 90% -.- 30% set point 100% -.- 30% So it sets level to half of required level until 30% level has been reached. I don't get what the problem is. ------------------------------------------------------------------------------------------ |
Last edited by: svud at: 4/22/2016 2:21:51 PMLast edited by: Min_Moderator at: 4/25/2016 8:59:56 AMNew subject after splitting Last edited by: Min_Moderator at: 4/25/2016 9:02:07 AMSplit from other thread |
|
4/22/2016 6:03 PM | |
Joined: 5/28/2008 Last visit: 9/3/2025 Posts: 4522 Rating:
|
Hello, Please have a look on this valuable tip from Expert hdhosseini Implementing complex loop configuration with PID controllers |
Ayman Elotaify |
|
This contribution was helpful to
2 thankful Users |
4/25/2016 9:46 AM | |
Joined: 11/21/2007 Last visit: 7/25/2025 Posts: 2326 Rating:
|
Hello Your application is Similar to Steam Drum Level Control. This application basically consists of two interlinked loops. 1. Outlet Flow Loop ( Normal PID ) 2. Level Loop - ( PID with additional Feed-Forward Gain ). ( Add the actual Flow of Outlet Flow Loop as Feedforward Gain ) The Attached Application note will help you understand the application Hope this helps Cheers Navnag
AttachmentYS1700_Drum_Level_Control.pdf (407 Downloads) |
Last edited by: Navnag at: 4/25/2016 9:47:16 AMThere is no such thing as the last bug in a program |
|
This contribution was helpful to
2 thankful Users |
Follow us on