(0)| 6/14/2016 8:54 AM | |
|
Posts: 16 Rating:
|
i have two generator 1000 kva g1 and 1000kva g2 same specifics i need to connected them in paraller so first the g1on and when the load is high the g2 on auto and when the load is low the g2 it is off auto can any one help me plc programs7-200 program in ladder any one help me ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 6/14/2016 9:51:36 AMNew subject after splitting Last edited by: erwwq at: 6/16/2016 11:08:02 AMLast edited by: erwwq at: 7/5/2016 2:09:23 AM |
|
Follow us on