(0)| 8/8/2016 9:08 AM | |
|
Posts: 2 Rating:
|
I am having faults on my Profibus network, consisting of a fiber optic ring with several OLMs, and drops off each OLM are Supermicro softPLCs (CP Card). The network consists of 12 Nodes & the distance between each OLM is ~10meters I checked the installation: Copper cables, connectors all found to be good. There are no power cables or VFD drives is the vicinity of the Profibus cables. I connected up the Profitrace adapter to analyse & found reqular station loss & retries on several devices. Each drops from the OLM is more than 2 meters. In Profitarce Software, what i did notice was the transmission speed, set at the maximum of 12MB/s. I dont think it is nescessary to run at that high rate & this may be the cause of these comms faults. Can somebody assist me? ------------------------------------------------------------------------------------------ Attachment4357003.pdf (315 Downloads) |
Last edited by: Min_Moderator at: 8/8/2016 2:58:22 PMNew subject after splitting |
|
| 8/8/2016 2:59 PM | |
|
Posts: 4757 Rating:
|
The second thread is published with the subject Faults on Profibus network, possible to reduce the speed? within the conference Communication / Networks. Greetings |
Follow us on