(0)| 10/9/2016 5:49 PM | |
|
Joined: 9/23/2005 Last visit: 1/8/2026 Posts: 4440 Rating:
|
“Simple Samples” are small projects that demonstrate simple features. The target is give a quick overview about the theme and be used as start point for related discussions. Follow there are a short description and the configuration main steps. Description: in this simple sample, controller FB variables are automatically created on HMI tag table. Requirements: TIA V14 SiVArc (SIMATIC Visualization Architect) Project with a minimum configuration: S7-1500 configuration, Configuration main steps:
Result: on WinCC Application → HMI tags a “Data_block_1” tag table was created with the related controller instance DB variables (Data_Block_1_on, Data_Block_1_Status) References: TIA Portal online help: Help → Show help contends → SIMATIC Visualization Architect Project: Due a size/ format restrictions, the projects (one before and one after SiVArc generation) were first archived as zap14 format and after that attached to a zip archive (.zip). AttachmentProjects.zip (208 Downloads) |
|
Denilson Pegaia |
|
| 10/14/2016 1:41 PM | |
|
Posts: 4757 Rating:
|
New question published by Jason G is split to a separate thread with the subject Simatic Visualization Architect v2.0 needed. Best regards |
Follow us on