10/16/2016 8:38 AM | |
Posts: 9 Rating:
|
Good morning I saw this post and wanted to know if anyone has a comprehensive description of how to use the backlights that I can read. I wanted to know 1. How many colors are available? 2. Is it possible to get the display to flash or alternate between colors Etc ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 10/17/2016 11:27:33 AMNew subject after splitting |
|
10/16/2016 9:05 AM | |
Joined: 12/18/2014 Last visit: 9/12/2024 Posts: 33755 Rating:
|
Backlight flags: Flags M25, M28 and M29 control the backlight of the LOGO! onboard display. Flags M26, M30 and M31 control the backlight of the LOGO! TDE. You can use the outputs of timers, message texts, or other function blocks to activate the backlight flags. To enable multiple conditions to control the backlight of the devices, you can use multiple function blocks in parallel or in sequence. M25 = LOGO! displays white backlight. If backlight flags are connected in parallel, the color of the flag which has the higher number is activated. If the markers M25, M28 or M29 are used in the program, the onboard backlighting of the LOGO! when pressing the cursor keys, you will no longer be automatically activated. Look at attachment. AttachmentBacklight_test.zip (303 Downloads) |
Follow us on