(0)| 10/24/2016 7:17 PM | |
|
Posts: 3 Rating:
|
Hello. I have the same problem. I try to backup a TP177A via "PC ADAPTER USB A2" cable and by using ProSave ver7.4.6.0 and does not work.I set the ProSave to MPI/DP address 1, but does not communicate with TP177A. The TP177A is in transfer mode. Any suggestions? ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 10/25/2016 4:24:43 PMNew subject after splitting |
|
| 10/25/2016 12:59 PM | |
|
Posts: 3 Rating:
|
Finally i managed to backup the TP177A via the PC adapter USB A2 cable. I had to set the Pc adapter to MPI mode , instead of AUTO which is the default setting. |
| 3/23/2018 2:44 PM | |
|
Posts: 63 Rating:
|
Have you selected the transfer mode on the panel itself? this will activate the communication to the panel. |
Follow us on