(0)| 11/9/2016 5:25 PM | |
|
Posts: 1 Rating:
|
Hello my name is David. I have the same problem with DTM LR250 HART, Not working in PACTware 5.0 neither Fieldmate 3.0. For me, is rare that error appears in twice filed software, "The sitrans DTM needs at leas one installed device description to function properly". "Please install the missing device description(s) before trying to use dtm". Please help me with this issue, I need to do commissioning of several devices sitrans. Thanks. ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 11/9/2016 6:36:37 PMNew subject after splitting |
|
| 5/27/2018 7:50 AM | |
|
Posts: 12 Rating:
|
Hello, Siemens DTM files are based on EDD, so the Siemens DTM files to work on a platform like PACTWARE need an interface which is SITRANS DTM software that should be installed before installing DTM files. SITRANS DTM: https://support.industry.siemens.com/cs/ww/en/view/47512455
|
Last edited by: Jen_Moderator at: 5/28/2018 10:04:32 AMOptimized link. |
|
Follow us on