(1)| 2/24/2017 12:57 PM | |
|
Joined: 9/2/2012 Last visit: 9/25/2025 Posts: 712 Rating:
|
Hi, I wanted to do chinese(taiwan) language in TP1500 Comfort. Project settings are done as per manual and working ok in simulator on PC. But in HMI its shows as "square box" instead of actual actual text. Which "font" i need to select in runtime selection ? Also do i need to install any language to HMI via prosave/hmi maintenance option ? If so where can i get "taiwanese" language file ? I could able to see only chinese,korean,japanese under tha path- C:\Program Files (x86)\Common Files\Siemens\PTProSave\AddOn In case any other language required and not available in "addon" what is the procedure? ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 2/24/2017 3:03:47 PMNew subject after splitting
|
|
| 2/24/2017 3:01 PM | |
|
Joined: 8/3/2009 Last visit: 1/9/2026 Posts: 16629 Rating:
|
Hello Minsuu I think the font is Simsun Here is an older FAQ but it shows the needed Font: https://support.industry.siemens.com/cs/ww/en/view/28878919 |
|
If this Information really helps, you could use the Rate function |
|
| 2/28/2017 10:15 AM | |
|
Joined: 8/3/2009 Last visit: 1/9/2026 Posts: 16629 Rating:
|
Hello Now I have found also this FAQ: How do you clear display problems with Chinese characters on Comfort Panels?https://support.industry.siemens.com/cs/ww/en/view/99050732 I think this is the right one for you!!!!! Good luck! Bye Murof |
|
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to
|
|
| 3/1/2017 9:19 AM | |
|
Joined: 9/2/2012 Last visit: 9/25/2025 Posts: 712 Rating:
|
Dear Murof, Thank you for the answers and links. There was some confusion / mistake from my side to understand the requirement. Basically i was trying with chinese (taiwan) language instead of THAI language. "chinese (taiwan)" is working ok with the font "MingLiU" Now if am trying for THAI language, it is not working by default. So i got information from my colleague that the font option of all the text in the project where need this language switching should support both the language. That is if i configured required font under "configured font" also entire project text font will be as per default font. which may not be supported by all the language. So we need to update the font in all the screen manually. After setting he "configured font" as per requirement, i configured the same font for "default font" also. But the project text is not changing. So i changed everything manually and found working. Please see the attachment. AttachmentHMI LANGUAGE.pdf (1023 Downloads) |
|
|
|
Follow us on